2025-01-22 4:54 PM
I am using the STM32H7B3I-DK and trying to read and write from an SD card using SDMMC1 with TouchGFX running (also FreeRTOS). I have solved a NO_FILESYSTEM ERROR described here. While this allowed me to mount, open, and write to a file, I still get NO_FILESYSTEM Error on reads from the card.
Additionally I have noticed the following line is a defining line that allows the SDCARD to mount, open, and write; however, it also leads to my display flickering in many areas when updating.
MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;Can someone help me understand what may be going on here regarding the read Error and how the MPU settings are causing the flicker?
The following is my MPU Code and regions defined in linker file:
void MPU_Config(void)
{
MPU_Region_InitTypeDef MPU_InitStruct = {0};
/* Disables the MPU */
HAL_MPU_Disable();
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Enable = MPU_REGION_ENABLE;
MPU_InitStruct.Number = MPU_REGION_NUMBER0;
MPU_InitStruct.BaseAddress = 0x90000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_256MB;
MPU_InitStruct.SubRegionDisable = 0x0;
MPU_InitStruct.TypeExtField = MPU_TEX_LEVEL0;
MPU_InitStruct.AccessPermission = MPU_REGION_NO_ACCESS;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_DISABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_NOT_SHAREABLE;
MPU_InitStruct.IsCacheable = MPU_ACCESS_NOT_CACHEABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_NOT_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Number = MPU_REGION_NUMBER1;
MPU_InitStruct.Size = MPU_REGION_SIZE_64MB;
MPU_InitStruct.AccessPermission = MPU_REGION_FULL_ACCESS;
MPU_InitStruct.IsCacheable = MPU_ACCESS_CACHEABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Number = MPU_REGION_NUMBER2;
MPU_InitStruct.BaseAddress = 0x24000000;
MPU_InitStruct.Size = MPU_REGION_SIZE_1MB;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/** Initializes and configures the Region and the memory to be protected
*/
MPU_InitStruct.Number = MPU_REGION_NUMBER3;
MPU_InitStruct.Size = MPU_REGION_SIZE_256KB;
MPU_InitStruct.DisableExec = MPU_INSTRUCTION_ACCESS_ENABLE;
MPU_InitStruct.IsShareable = MPU_ACCESS_SHAREABLE;
MPU_InitStruct.IsBufferable = MPU_ACCESS_BUFFERABLE;
HAL_MPU_ConfigRegion(&MPU_InitStruct);
/* Enables the MPU */
HAL_MPU_Enable(MPU_PRIVILEGED_DEFAULT);
}
//Linker File
MEMORY
{
DTCMRAM (xrw) : ORIGIN = 0x20000000, LENGTH = 128K
ITCMRAM (xrw) : ORIGIN = 0x00000000, LENGTH = 64K
RAM (xrw) : ORIGIN = 0x24000000, LENGTH = 256K
RAMFB (xrw) : ORIGIN = 0x24040000, LENGTH = 768K
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 2048K
OSPI (xrw) : ORIGIN = 0x90000000, LENGTH = 64M
SDRAM (xrw) : ORIGIN = 0xD0000000, LENGTH = 8M
}
Thank you!
2025-01-23 1:19 AM
hello @EthanMankins ,
Please try the TouchGFX Demonstrations for the STM32H7B3I-DK available in our STM32CubeH7 FW , You can find them on ST.com V1.12.0 under this path : Firmware\Projects\STM32H7B3I-DK\Demonstrations\TouchGFX.
These examples might help solve your problem.
Regards .
2025-01-23 9:50 AM
@MOBEJ Thank you for you suggestion. I am having trouble finding an example with an SD card and TouchGFX that would relate to my issue.