STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H755 USB CDC Help

Hi everyone, I’d like to ask for your expertise. I’m working with a custom board based on the STM32H755ZIT, configured in LDO mode. My issue is that when I connect the board to my PC via USB to use the Virtual COM Port (VCP), the computer does not de...

Resolved! USB PD Extended Source Capabilities

Hi,How do I serve request Get Source Capabilities Extended? I'm using STM32G0B1 with a port configured as SRC.When a SINK sends the Get Source Capabilities Extended the STM PD library responds with 'Not Supported' and my code is not aware that this e...

Mulleteer_0-1776944660689.png

Resolved! Possible bug in HAL_UART_DeInit()

Hello all,There might be a possible bug in HAL_UART_DeInit(). When calling HAL_UART_DeInit() when it is already initialized could lead to CPU starvation. Assume that an interrupt fires after calling __HAL_UART_DISABLE(huart); and before huart->Instan...

bala- by Associate II
  • 717 Views
  • 4 replies
  • 1 kudos

bootloader for lpuart

is there a template for developing a custom bootloader that uses the lpuart?Has the application firmware the ability to trigger a bootloader state so I can upload the new application firmware into stm32g051g8?What are the changes that I have to do on...

Awful timeout implementation in SDMMC

SDMMC HAL driver implementation is full of timeouts like this:uint32_t count = SDMMC_CMDTIMEOUT * (SystemCoreClock / 8U / 1000U); do { if (count-- == 0U) { return SDMMC_ERROR_TIMEOUT; } sta_reg = SDMMCx->STA; } while (SOME_FLAG_NOT_SET);I...