STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Arbitrary waveform by timer using DMA

Hello,I want to generate an arbitrary waveform by a timer using DMA. The waveform is using different pulse widths and also varying periods in multiples of 25µs.By reading AN4776 and HAL documentation I figured out it should be possible with HAL_TIM_D...

RAltm by Senior
  • 514 Views
  • 14 replies
  • 2 kudos

STM32F4 + DP83848: Ethernet not working

I am a beginner in electronics. I recently designed a board using the STM32F407VGT6 and DP83848, but after assembly and testing, I encountered a problem.  The board can be programmed and it runs, but the Ethernet section does not work properly.  It d...

Optimizer problem with USBPD

Hi, I have an USBPD sink application created with CubeMX that can be found here:https://github.com/ThiRom/H563NucleoUSBPDSink   The project can be build using cmake. If the project is build using Debug configuration, it works. But using Release it sh...

USBPD.png
RomThi by Associate III
  • 438 Views
  • 8 replies
  • 1 kudos

GPDMA in Linked List with OCTOSPI

Hi all !I'm trying to write a driver for a LevelX system to talk to a QSPI chip over the OCTOSPI1 peripheral (STM32H563). I got the chip to respond to most commands, set it up in reading / protected mode.But, later, I've spotted an issue : I cannot s...

lheywang by Associate
  • 158 Views
  • 2 replies
  • 0 kudos

EPR request in STM32G071

HelloI have my own board with STM32G071KBT6 microcontroller. I successfully comunicate with charger by PD protocol and I receive up to 21 V (PPS). But I need above 21V. I have power bank with AVS up to 28V and USB cable with e-marker (up to 240W). Ho...