STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H7 LWIP cache bug + fix

Posted on March 26, 2018 at 12:54 I have a Nucleo-H743ZI board that I'm running some ethernet code on, that I based on the LWIP example applications. The problem was that I could only ping it once on every reset. The problem went away when I disa...

Resolved! UART DR vs TDR/RDR registers

Posted on April 16, 2018 at 17:30I don't understand something, what's the point of TDR and RDR registers if during the Receive and Transmit functions they read/write into the DR register.Moreover UART is normally full duplex but if we read/write int...

oldone by Associate II
  • 6884 Views
  • 7 replies
  • 0 kudos

image on lwip http server

Posted on April 16, 2018 at 16:33I ve been messing around with the http server example (netconn) of the lwip stack in stm32f4 dev board. the example works well and I see the example web page without probles. The problem apears when I change the web ...

Resolved! Porting of X-CUBE-CLD-GEN to NUCLEO-L4R5ZI

Posted on April 13, 2018 at 09:21Hi Team,I have downloaded the package X-CUBE-CLD-GEN, i want to port tohttp://www.st.com/en/evaluation-tools/nucleo-l4r5zi.html, i want to know what are the changes i need to do. I'm using Atollic IDE.i want to under...

STM32F072 IAP solution

Posted on April 16, 2018 at 13:47Hello EverybodyI'm new in this Community and I hope to find ideas to solve my problem: I've an application in which I deal with a phone via a tag and I2C. I store an image of the new firmware I've to write to microco...

SVD files of STM32F7

Posted on April 14, 2018 at 14:01Hi,I am working with the http://www.st.com/en/microcontrollers/stm32f767zi.html microcontroller using the GNU ARM embedded toolchain.Since I didn't want to work with the CMSIS library I only copied a few header files...

NUCLEO-F767ZI USB Virtual COM Issue with CubeMx

Posted on April 13, 2018 at 01:44Hello,I am trying to get a basic USB CDC virtual COM program working using the NUCLEO-F767ZI with CubeMx (v4.23.0 and F7 v1.8.0) but facing an issue where my Windows 10 keeps messaging me that the USB device is not r...