Skip to main content
Tom Schrauf
Associate II
May 24, 2018
Question

STM32F103 bootloader starting conditions

  • May 24, 2018
  • 2 replies
  • 831 views
Posted on May 25, 2018 at 00:16

Hi,

I'm using a STM32F103C8T which shall be in circuit programmed by an ESP8266.

For this reason i connected PA9/PA10 to the USART Port of the ESP and the ESP controls Reset and BOOT0 to start the STM32 in Boot or Run mode.

When sending the Sync-Character the STM was not synchronizing and did not respond. After hours of searching i found out that i had to remove external 4K7 pullups attached to PB8 and PB9. Only after that the STM was willing to talk but I did not find any explanation.

45  - PB8 I/O FT PB8 TIM4_CH3(9) I2C1_SCL / CANRX

46  - PB9 I/O FT PB9 TIM4_CH4(9) I2C1_SDA/ CANTX

According to AN2606 the Medium-density STM32F103 only supports USART (V2.2).

CAN is supported for the Connectivity line devices only so I have no clue why high levels on PB8/PB9 are blocking the USART-Bootloader.

What did i forget to read or did something else block my bootloader and I blamed PB8/9 by mistake?

Thanks for your support !

#stm32-uart-bootloader
This topic has been closed for replies.

2 replies

waclawek.jan
Super User
May 24, 2018
Posted on May 25, 2018 at 00:44

If you put back one or both pullups, will it stop talking again?

JW

Tom Schrauf
Associate II
May 25, 2018
Posted on May 25, 2018 at 10:30

It was a problem of the ESP (sharing i2C) together with a high BOOT1 pin.

THANK YOU and sorry for bothering but sometimes one thinks into the wrong direction. As a penalty i un/resoldered two STM32 chips ;)