STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Use to flash memory for binary for data save

Posted on June 07, 2018 at 09:16Hi.Now, I can unlock flash memory for data save by erase page size 800(2kbyte) and I would like to data save for binary.Example 0x0800800 for '1'0x0800801 for '2'0x0800802 for '3'How should I do?below my code for eras...

Gz by Senior
  • 773 Views
  • 0 replies
  • 0 kudos

Does the STMF103 USB support a promiscuous mode?

Posted on February 07, 2018 at 08:41Hey,I want to implement a �smart USB hub� (in software) which will include multiple devices, not a single compound device. Currently I can set the device address with the relevant register and get only the transac...

ITM usage and SWO pin

Posted on June 06, 2018 at 10:25Good morning,I am trying to add some trace capabilities to my system: UART is obviously too slow so I would like to use ITM. I report my situation:I use a STM32F3DISCO board, FreeRTOS, Eclipse with Jlink debugger plug...

STM32L432KC RTC Init Fails after DFU

Posted on February 15, 2017 at 04:36 I created a PCB based on the STM32L432KC. It uses an LSE for the RTC. I am using STMCubeMX 4.0 to create the initialization code with version 1.6.0 of the STM32L4 HAL library. The system starts up fine from...

STM32F103 CAN IT won't retrigger

Posted on June 05, 2018 at 09:20Hello everyone, I am having a little issue with my STM32F103RBT6 code. I am trying to make the Receive CAN IT work.The problem I am facing is that it is working for a small amount of time and then just stops (either i...

B C by Associate II
  • 902 Views
  • 1 replies
  • 0 kudos

STM32F437 Ethernet does not sent packets

Posted on June 04, 2018 at 20:42Hello,I have an ownmade ethernet board having Micrel/Microchip KSZ8081MNX.I started using NUcleo STM32F429ZI using CubeMX 4.25.1At first it all looked promising and could identify the places where to change the settin...

taraben by Senior
  • 910 Views
  • 0 replies
  • 0 kudos