STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Transferring 100Mbit/sec from STM32F76x to PC

Hi,We need to transfer big amount of data from an STM32F76x connected to a PC. The expected transfer rate of data is 100Mbit/sec (100 mega bit per second). Few basic questionsis it possible to transfer in such rates?can\should it be done over LWIP?ca...

Using PDM to PCM conversion library

I am using a STM32L1 MCU and I want to use the PDM to PCM conversion library, so I downloaded X-CUBE-MEMSMIC1, in the audio PDM lib folder I found libPDMFilter_CM3_Keil.lib. In the release note I read this lib is for 16KHz PCM data sampling rate, So ...

J Lee by Associate III
  • 5021 Views
  • 4 replies
  • 0 kudos

Resolved! STM32L4 USB PID Allocation for consumer product

Hi,I am working on a consumer product based on STM32L4 microcontroller and need to register a new PID before we start shipping. Appreciate some assistance.Similar threads:https://community.st.com/s/question/0D50X00009XkXJESA3/help-needed-with-usb-pi...

CPatr by Associate
  • 1842 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F042 Bootloader Activation

Hy, I am planning a system where 2 STM32F042 UFQFPN28 devices serve as CAN Controller and are controlled by one master CPU. PCB Space and CPU pins are short. I need to guarantee a fail safe FW update for the two STM32 MCUs.I plan to wire the system a...

0690X000006CGl8QAG.png 0690X000006CGlIQAW.png
harald by Associate III
  • 2022 Views
  • 4 replies
  • 1 kudos

Any USB examples for the NUCLEO-H743ZI board?

I could not find any in the Cube packages... I tried creating a project from scratch with STM32CubeMX. Power for USB FS1 is ready (LD10 on) but no reaction at all when I connect anything via user USB port (CN13). The same project works on the STM32H7...

Microman by Associate III
  • 1298 Views
  • 2 replies
  • 0 kudos

STM32F103C8 USB Unknown Device Problem

Posted on July 27, 2017 at 15:51Hi friendsI am trying to make usb hid connection with STM32F103C8. I was able to compile the USB Library via the KEIL Compiler. The processor is running. After the USB init routines, the processor goes to the main pro...

0690X00000603ywQAA.jpg

USB device not enumerating sometimes

Posted on January 06, 2015 at 08:13We are using STM32L151CBU6 in our product development and need to connect the device to PC over USB. I have used the USB driver provided by ST. I am seeing a really strange and frustrating behavior. From the IAR de...

pankaj1 by Associate
  • 1394 Views
  • 1 replies
  • 0 kudos