STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Switching between thread on RTOS ?

Posted on March 29, 2017 at 04:18Everybody,I want to switch between thread on RTOS, how can I do that ?I've written down below, but it seems that it's staying on the first thread only,Thanks/* StartDefaultTask function */void StartDefaultTask(void c...

Resolved! SD with DMA works, except in callback

Hey everyone,I'm seeing something weird.I've got a working SDIO in 4 bit mode, with dma (FIFO enabled with peripheral flow controller) and using a stm32f722ze.It works perfectly. I can write a large bunch of data to the SDcard relatively quickly even...

con3 by Senior
  • 2012 Views
  • 4 replies
  • 0 kudos

STM32F091CBT6 BootLoader application problem. After jumping to main application from bootloaer, timer interrupt didn't work.

STM32F091CBT6 BootLoader application problemIn the bootloader, there is no ploblem and jump to application code exactly. If I jump to application firmware in main() routine, timer interrupt works well, but if I jump to application firmware in sub-rou...

BYOO by Associate II
  • 3199 Views
  • 7 replies
  • 0 kudos

STM32L4 + STM32CubeMX + CMSIS-RTOS

Hello,I am using my STM32L4R5 with CMSIS RTOS generated from STM32CubeMX. I followed the example and I wrote a program that wakes the CPU up from sleep mode every time I press the button (external interrupt)/* USER CODE END PD */   /* Private macro -...

Duy Tran by Associate II
  • 1106 Views
  • 0 replies
  • 0 kudos

STM32F072 USBD_LL_Transmit problem

Posted on July 01, 2016 at 11:04I'm using STM32F072 MCU in USB Device mode. The USB enumerates nicely creating 1 interface and 2 bulk endpoints. One input and one output. Both with the maximum transfer size 64 bytes.The problem occurs when I try to ...