cancel
Showing results for 
Search instead for 
Did you mean: 

It seems like bug detected in HAL library for STM32F103C8 (bluepill) board.

sfrwmaker
Associate II

I am trying to create PWM signal using DMA channel using circular buffer. TIM2, channel1, DMA1_channel5.

I have created the configuration using CubeMX. Then I have investigated the HAL_DMA_IRQHandler() procedure called by DMA1_Channel5_IRQHandler().

If I register FULL BUFFER callback using HAL_DMA_RegisterCallback(&hdma_tim2_ch1, HAL_DMA_XFER_CPLT_CB_ID, <some CB>), it overwrites with system TIM-blah-blah callback and my callback never fires!

If HAL_DMA_RegisterCallback(&hdma_tim2_ch1, HAL_DMA_XFER_HALFCPLT_CB_ID, <some CB>) does not called prior HAL_TIM_PWM_Start_DMA(&htim2, TIM_CHANNEL_1, (uint32_t *)data, LEN),

NO HALF BUFFER interrupts fires at all. I mean the corresponding section in the HAL_DMA_IRQHandler() does not work.

How can i make sure my routines be fired when half buffer and full buffer transfer complete?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0