cancel
Showing results for 
Search instead for 
Did you mean: 

I have some problem about STM32429zi-disc1 card usart2 periph

RageLog
Associate

I have some problem about STM32429zi-disc1 card usart2 periph. I'm sending data via usb to rs232 conv but data is wrong. In my opinion, boud rate is different from my choice. probably, its derive from PLL. How can I fix it ? Pc always receive 0x00 or similar data

My PLL setting is following:

************************* PLL Parameters *************************************/

/* PLL_VCO = (HSE_VALUE or HSI_VALUE / PLL_M) * PLL_N */

#define PLL_M 8

/* USB OTG FS, SDIO and RNG Clock = PLL_VCO / PLLQ */

#define PLL_Q 7

#if defined (STM32F40_41xxx)

#define PLL_N 336

/* SYSCLK = PLL_VCO / PLL_P */

#define PLL_P 2

#endif /* STM32F40_41xxx */

#if defined (STM32F427_437xx) || defined (STM32F429_439xx)

#define PLL_N 360

/* SYSCLK = PLL_VCO / PLL_P */

#define PLL_P 2

#endif /* STM32F427_437x || STM32F429_439xx */

#if defined (STM32F401xx)

#define PLL_N 336

/* SYSCLK = PLL_VCO / PLL_P */

#define PLL_P 4

#endif /* STM32F401xx */

and my usart code is following:

USART_InitStruct.USART_BaudRate = 115200;

USART_InitStruct.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

USART_InitStruct.USART_Mode = USART_Mode_Rx|USART_Mode_Tx;

USART_InitStruct.USART_Parity = USART_Parity_No;

USART_InitStruct.USART_StopBits = USART_StopBits_1;

USART_InitStruct.USART_WordLength = USART_WordLength_8b;

USART_Init(USART2,&USART_InitStruct);

USART_Cmd(USART2,ENABLE);

InitGPIO( sGPIOD,

GPIO_Mode_AF,

GPIO_OType_PP,

GPIO_Speed_100MHz,

GPIO_PuPd_UP,

GPIO_Pin_5|GPIO_Pin_6);

GPIO_PinAFConfig(GPIOD,GPIO_PinSource5,GPIO_AF_USART2);

GPIO_PinAFConfig(GPIOD,GPIO_PinSource6,GPIO_AF_USART2);

main loop is :

while(1){

while(!USART_GetFlagStatus(USART2, USART_FLAG_TXE));

USART2->DR = 0x0002;

_delay_ms(1000);

}//EOF Loop

My usart converter is profilic and ch34. Ist work another my desktop app

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0