STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FATFS ERROR ( f_opendir) with FreeRTOS

Hi All,​I`m trying to build a project using STM32CubeMX with FreeRTOS and have FatFS for my own Board.And when I execute the code,it can {f_mount} really well but till {f_opendir} it come out the FR_INT_ERR.​I have a question about if I use the FreeR...

0690X00000AA4ZFQA1.png 0690X00000AA4ZUQA1.png

stm32 c2c iam getting errors

iam getting following error when i am trying to connect with grovestream iam using en.xcubec-cld-genfollowing are theerrors iam getting***** Grovestreams HTTP Cloud application *****Opening connection to server grovestreams.com.H:/TRIAL/STM32CubeExpa...

DPADI.8 by Associate II
  • 1210 Views
  • 2 replies
  • 2 kudos

Updated firmware(through usb pendrive) hangs

 I am working on a project in which i have to upgrade the firmware using a usb key on stm32f07 discovery board. the firmware upgrade is successful and some blinky codes are working. but when i upload the code with sd card driver and usb host driver ...

nucleof103rbt6 HAL CAN receiver interrupt not firing

Hi ,i am notable to get the can receive interrupt to fire .using hal libraries. code sample attached.i have previously used the CAN on the bluepill with stdperipheral libraries.Kindly help.UPDATE:i have checked the sfrs with ESR having REC=FF, EFVP &...

Hp.14 by Associate II
  • 1385 Views
  • 2 replies
  • 0 kudos

How to create STM32F407G-DISC1 intercom system?

Hi! I am trying to create an intercom system with STM32F407G-DISC1 boars, where one speaks and every listen. I am little bit confused about how to configure cs43l22 codec and if this concept will work. Or it is better to create PDM bus?Thank you.

0690X00000A9whaQAB.png
s.kirill by Associate II
  • 1996 Views
  • 3 replies
  • 0 kudos

[Bug] Undefined behavior in LL_ADC_SetChannelSingleDiff causes it to alway set bits in gcc and clang

From LL_ADC_SetChannelSingleDiff: /* Bits of channels in single or differential mode are set only for        */ /* differential mode (for single mode, mask of bits allowed to be set is   */ /* shifted out of range of bits of channels in single or dif...

I am trying to program the main memory using Demonstrator GUI application. But i am getting below attached error. PLease help me to get use of system bootloader.

i am using Neucleo L4R5ZIP development board. I am planning to use System Bootloader. I have enabled the system bootloader by enabling the BOOT0 pin and BOOT1 Register configuration. Through LD3 LED, i can able to verify the system Bootloader started...

Kmoor by Associate
  • 914 Views
  • 0 replies
  • 0 kudos