2018-07-04 11:10 PM
Hi everyone, in my system (freertos based) i need some low pulse before sending uart datas. So i must change tx pin to gpio and send low pulse along appx. 100uS and after that i must rechange it to uart fastly. How can i do this dynamically and time efficently. I need an advice for it. Thanks.
#freertos #uart #gpio2018-07-05 12:07 AM
Hello
ILTAR.Ismail_Fatih
,take a look in reference manual for GPIO_MODER register. You may change between output and alternate function mode and configure pin state (when in output mode) using GPIO_ODR register.
2018-07-05 2:57 AM
I just tried something like that but uart tx pin always stays at reset state. ıt doesnt send any datas.
#define tim2_wait_usec(X) \
TIM2->PSC = 71; \
TIM2->ARR = X; \
TIM2->CNT = 0; \
TIM2->CR1 |= TIM_CR1_CEN; \
while (TIM2->CNT != TIM2->ARR) { } \
TIM2->CR1 &= ~TIM_CR1_CEN
void MX_GPIO_uart1tx_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
GPIO_InitStruct.Pin = GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
void MX_GPIO_uart1tx_deInit(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
GPIO_InitStruct.Pin = GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_PULLUP;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
void send(uint8_t* buffer, uint16_t size)
{
MX_GPIO_uart1tx_Init();
HAL_GPIO_WritePin(GPIOA, GPIO_PIN_9, GPIO_PIN_RESET);
tim2_wait_usec(100);
MX_GPIO_uart1tx_deInit();
MX_USART1_UART_Init();
HAL_UART_Transmit_IT(&huart1, buffer,size+1);
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
2018-07-05 3:52 AM
You have to fill out all fields of the
GPIO_InitTypeDef struct.
JW
2018-07-05 4:05 AM
i simplified codes and filled out all fields (just speed neccessary). and it still hangs at low states
void MX_GPIO_uart1tx_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
GPIO_InitStruct.Pin = GPIO_PIN_9;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_PULLDOWN;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF7_USART1; //not used
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
}
void send(..)
{
MX_GPIO_uart1tx_Init();
osDelay(1);
MX_USART1_UART_Init(); //cubemx generated default uart init
HAL_UART_Transmit_IT(&huart1, buffer,size+1);
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
2018-07-05 8:36 AM
i have done with below code. ı had to add USART deinit before gpio init but i dont know the reason exactly. And this method is not fast and efficent in my opinion. Still need a best way
void send(..)
{
HAL_UART_DeInit(&huart1);
MX_GPIO_uart1tx_Init();
tim2_wait_usec(100);
MX_USART1_UART_Init();
HAL_UART_Transmit_IT(&huart1, buffer,size+1);
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.