STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LAN9353 using STM32H743

Edited by a ST moderator: Please kindly don't use capital letter as it gives the impression of "shouting" Hi Team, I am using stm32h743 to interface lan9353 (3 port ic). for the first step if i connect one end of the ethernet cable to board and anoth...

Vani_123 by Associate II
  • 444 Views
  • 1 replies
  • 0 kudos

Timer using DMA

HiI currently use a timer in interrupt mode that triggers every 50 µs and executes my function inside HAL_TIM_PeriodElapsedCallback. I also have another timer running every 1 second. To reduce CPU load, I want to replace the 50 µs interrupt-based tim...

avbST by Associate II
  • 485 Views
  • 1 replies
  • 0 kudos

STM32H723 PSSI DMA

Post edited by ST moderator to be inline with the community rules for the code sharing. In next time please use </> button to paste your code. Please read this post: How to insert source code. Hello,   i have a Project, where i have an FPGA connected...

STM32 ISP-IQTune Port Detection Issue with IMX335 on STM32N657X0H3Q

大家好!问题是这样的: 我正在尝试使用 STM32 ISP-IQTune 应用程序通过 STM32N657X0H3Q 板读取 PC 上的 IMX335 相机数据。但是,IQTune 无法检测到任何可用的 COM 端口。这是我的设置:硬件:板:STM32N657X0H3Q相机:IMX335(MB1854B模块,根据文档提供原生支持)。固件:已从 STM32N6 固件包中刷新 DCMIPP_ContinuousMode 示例。连接:已将板上的两个 USB 端口连接到 PC(USB-C 电缆)。开发板...

陶铸 by Associate II
  • 1831 Views
  • 5 replies
  • 0 kudos

FreeRTOS Tick Speed

Good evening,  I need freeRTOS tick speed to be greater than 1kHz, I tried to change the configTICK_RATE_HZ parameter but get a divby0 error which I can't fix. Is there a way garanteed way to achieve what im looking for? Thx in advance 

Jack_DB by Associate II
  • 424 Views
  • 2 replies
  • 1 kudos