STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Ethernet example for STM32H745I-DISCO

Hi All,I have a ST32H745I-DISCO and would like to use its Ethernet port. It has a LAN8740A PHY connected to the MII port. There seems to be no Ethernet example for the STM32H745I-DISCO in stm32cubeh7. Does anyone know of an example that uses STM32 ...

Ade1 by Associate II
  • 1807 Views
  • 2 replies
  • 0 kudos

I want to send data from my Nucleo board to Matlab using the USB interface with the CDC protocol. But I am not able to open the port. What can I do to use the virtual COM port?

Request for help with USB CDC interface(STM32F401 Can not open Virtual Port)I want to send data at about 5Mbit/s from my Nucleo board to Matlab using the USB interface with the CDC protocol. I have now managed to get the PC to recognize a "Serial USB...

MScha.1 by Associate II
  • 986 Views
  • 0 replies
  • 0 kudos

USB not working on STM32F302C8 board

We are developing a USB prototype based around STM32F302C8. I cannot get this device to enumerate on USB, using either my own firmware, or the ST examples in STM32Cube_FW_F3_V1.11.0\Projects\STM32F302R8-Nucleo\Applications\USB_DeviceThere is some act...

PMcNe.1 by Associate
  • 635 Views
  • 0 replies
  • 0 kudos

USB Audio - Error code 43

Hi,I have implemented USB audio (on my project) which is based on the memsmic1 example project.The MCU i am using is STM32L496x, under keil IDE.the device is recogined by window as audio device but, when i disconnect and reconnect again, I am having ...

AA.10 by Associate III
  • 1096 Views
  • 2 replies
  • 0 kudos