STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Potential DAC and FreeRTOS conflict?

Hello,I am using STM32F417 to control a sounder among many other functions. In the firmware, the DAC is controlling the sounder which works fine when tested alone. However, the moment the FreeRTOS is enabled, the DAC stops working. What I am suspecti...

SKILA by Associate II
  • 2496 Views
  • 4 replies
  • 0 kudos

Trying to do arm_fft_fast_f32 256 bin for a 8000Hz sampled data. Taking only 8000 samples i.e. 1sec and diving into segments to do 256 fft. Not working after first iteration.

So dividing the sampled data and trying ti do each segment fft just like i did in matlab but the problem is the first segment fft is working next to that fft giving strange values. But if the second set/segment is done fft first it gives the right an...

AChan.3 by Associate
  • 909 Views
  • 0 replies
  • 0 kudos

STM32G4 IAP Bootloader Not Calling Application

Hi there,I need an IAP bootloader via CAN interface with G431 MCU. Before I had developed for F446 and no problem, and it works properly, no problem, but not for G4.The bootloader code has not called the application although set the stack pointer wit...

STM32F407 ethernet library

I wanna use Ethernet with STM32F407 MCU. I found only a standrad peripheral library on st.com site. Where can I get the official support library for Ethernet?

sminder by Associate II
  • 1569 Views
  • 2 replies
  • 0 kudos

CMSIS RTOS V1 : DSP and semaphore issues

Hi,I am using STM32F405, STM32Cube_FW_F4_V1.24.2, STM32CubeIDE, CMSIS RTOS V1, and CMSIS DSP library. I would like to use FFT and semaphores in my project.Does semaphore not work with CMSIS DSP? I know I can get semaphores as well as the DSP related ...

DLim.16 by Associate II
  • 2038 Views
  • 1 replies
  • 0 kudos

IAP over UART

Hello all,I know this has been probably done to death,but Just a quick link or some pointer if possible :I am using an ESP8266 to flash code to an STM32F103 over the UART.Basically I want to do what the "Flash Loader Demo" STM utlity does, by using t...

TFern by Associate III
  • 1759 Views
  • 2 replies
  • 0 kudos

STM32 MCUs IDE

Forwarded fromhttps://www.embedded-computing.com/home-page/rt-thread-iot-os-launches-rt-thread-studioRT-Thread has launched RT-Thread Studio, an integrated development environment for the open-source RT Thread IoT RTOS. A customized version of the Ec...

PPete.11 by Associate II
  • 967 Views
  • 1 replies
  • 1 kudos