STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB HID device enumeration and driver installation

Hello,I have a STM32F042 as USB HID Keyboard done with STM32CUBEIDE. Everything works nicly. Now here is my problem. If I plug the device into a running Windows PC for the first time the driver installation appears and all is fine. However if I plug ...

machinist by Associate III
  • 3175 Views
  • 6 replies
  • 0 kudos

DFU boot into NUCLEO-G431KB board.

I'm planning to build a custom board with the STM32G431KB on it and it needs to be programmed via USB.So I bought NUCLEO-G431KB board and soldered a USB cable on it.Red on VinBlack on GNDWhite on PA11 USB_DMGreen on PA12 USB_DPI also hooked PB8-boot ...

WSpar.1 by Associate III
  • 3744 Views
  • 8 replies
  • 0 kudos

Resolved! STM32 DFU USB CDC

Is it possible to do a DFU/SFU via USB CDC, how? On the UM2262 Applicate Note it mentioned on page 39 that local firmware download can be done through a UART Virtual COM port. I assume UART Virtual COM port is not the same as USB CDC. Appreciate your...

AAgar.2 by Associate III
  • 2161 Views
  • 7 replies
  • 0 kudos

Resolved! STM32 DFU Memory Requirements

How much memory should be available in the device flash to do the firmware install? If my application takes up >80% of my device's flash is it even possible to do a firmware update since most of the flash is already used up.Appreciate your support.

AAgar.2 by Associate III
  • 2570 Views
  • 6 replies
  • 0 kudos

Resolved! How to use HAL to leave the UART DMA in idle mode?

Hi,I'm trying to develop a module where information from a buffer is read by DMA and sent through UART, but the information is put in the buffer without a constant rate and it might happen that the buffer is empty, if that happened, I understand that...

mur by Associate III
  • 1705 Views
  • 2 replies
  • 0 kudos