2019-04-16 12:11 AM
My laptop act as server and my board (both the end are using statically configured IP) should receive the audio through Ethernet and store it on OTG USB drive.
2019-04-16 12:21 AM
I would use a plain TCP/IP connection.
Not aware of any higher-level streaming protocol implemented with LwIP.
Just keep irrelevant network traffic away, i.e. a ethernet adapter.
You will probably need some buffering scheme, to decouple ethernet reads from USB writes, and avoid stalls.
I don't understand the background. Why not storing the audio directly on the PC/laptop ?
Most projects are the other way around - the MCU streams real-time data to the PC.
2019-04-16 12:30 AM
I have to get real time audio through Ethernet and process it on board then revert to server(PC/laptop).
USB operation now not needed :)
If you have sample demo please share
Thanks in advance.
2019-04-16 1:03 AM
> If you have sample demo please share
Not my area of interest, sorry.
You will surely find several Cube examples for ethernet. Not sure if Cube is a good choice for hard real-time.
The F429 discovers doesn't seem to come with an ethernet phy.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.