Hello,
I try to upload my STM32 F446RE using bootloader through CAN. I get the STLINK V3SET and the utility STM32CuebeProgrammer. But the connection with the target is impossible.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-04-17 1:23 AM
I get few questionning:
- The STLINK does not detect any target voltage on the T_CAN_VCC pin, whereas I put 3.3V from my STM32 on it. What can I do ?
- The documentation says to put BOOT0 high and BOOT1 low. that's what I did. But connection's still impossible.. Do I have to let them high and low until I upload the microcontroller ? Or just few seconds in high and low state alow it to enter in bootloader mode ?
Maybe the second problem isn't really one because of the first blocking my handling. All I know is that is impossible to connect my target using STM32CubeProgrammer.
I would be grateful if anyone could help me to solve my problem.
Zephyr
Labels:
- Labels:
-
Bootloader
-
CAN
-
STM32F4 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0