STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! zephyr stm32u5g9j-dk2 adc not function

Hello, I am using the Zephyr operating system with the STM32U5G9J-DK2 hardware. I intend to collect voltage data using the ADC, but so far, no progress has been made. Here are the steps I have taken: I used the zephyr\samples\drivers\adc\adc_sequenc...

devin-hu by Associate II
  • 669 Views
  • 2 replies
  • 1 kudos

Resolved! STM32 - FileX and MSC - Windows read wrong data

Hi, I'm on a applicaiton involving USBX MSC and FileX. The final memory for the application is a NOR flash so I also use LevelX.Acutally, I'm working on a nucleo-U575ZI-Q without NOR flash so I use NOR Simulator on LevelX.My problem is that a file cr...

Dams_0-1760544703605.png
Dams by Associate III
  • 2657 Views
  • 20 replies
  • 1 kudos

NUCLEO-H563ZI Factory Demo Image

Hi. How can I build the Demo FW initially running on NUCLEO-H563ZI ?The is a number of projects in Cube under STM32Cube_FW_H5_V1.5.0\Projects\NUCLEO-H563ZI but it is not clear which one is the factory used to initially program the board. Thanks.  

dimax by Senior
  • 624 Views
  • 3 replies
  • 0 kudos

Resolved! Booting with dual flash banks vs. bank swap

Dear experts,I'm reading RMs for STM32 models with dual flash banks (F4, H7...) and don't quite understand how to use bank switching.Take the firmware update scenario when old firmware is in bank1 and new is programmed to bank2. So it programs some o...

Pavel A. by Super User
  • 16067 Views
  • 6 replies
  • 1 kudos