Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello,OSPI_RegularCmdTypeDef in stm32l4xx_hal_ospi.h doesn't include ".LatencyMode" member as below.how to set variable latency or fixed latency for Octo-SPI PSRAM on STM32L4P5G-DK board?Thanks. typedef struct{uint32_t OperationType; /*!< It indicate...
Hi All,I search for STM32 MCU discovery kit which meets the following conditions.・It have a 4-inch or larger LCD screen.・It have 10 or more GPIO ports that user can use freely.・It have 2 or more UART ports that user can use freely.STM32U5G9J-DK2 have...
As title says NUCLEO-H753ZI product page has no link to MB1364-H753ZI-E01 Schematics,only MB1364-H753ZI-C01.Second question, UM2407STM32H7 Nucleo-144 boards (MB1364)4.016 Oct 2023 has not mention NUH753ZI$AT3, only AT1 & AT2.
Hi all!First time poster.I'm working on a prototype that utilizes a Nucleo-G474RE to move some motors and read some sensors. The design is working great and my code is running as it should. However, recently I've been having some issues with the virt...
We are currently working on project, for which we are using the NUCLEO-G431RB development board. As we are now planning to move towards production of our devices, we require both the schematic and the Bill of Materials (BOM) for this board.I got sche...
Hello Community, Am interfacing LIS2DTW12 Acceleration Sensor with STM NucleoL476RGT6U by I2C communication protocal in blocking mode working everything fine. But i want collect data in non blocking mode so collecting data to DMA and implementing th...
Hello, my name is Matias from Efe Electrónica Argentina. I’m experiencing issues while programming my Riverdi 101STM32H7. Some of the problems include the device not being recognized and errors occurring when attempting to flash the memory using both...
Hi, I would be happy to consult,I am trying to implement the following with FREErtos and DMA NUCLEO-H743ZI2I want to receive packets sequentially on UART at some frequency.To parse the packets and then save only the valid ones for later use.What is t...
Hi all,I was looking at NUCLEO-U5A5 but I need support for TFT-LCD. TFT-LCD support is only available on the U599/U5A9 and better (see table below). There is also a NUCLEO-U575 but again no TFT-LCD support. Is there a plan to make a NUCLEO-U5xx with ...
Hi, I bough an STM32 F446RE and I have a USB cable mini-B but doesn't click with the board.Could you tell me what cable should I use?Should I use the mini-A?Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.