STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC - watchdog

@Amel NASRI @Tesla DeLorean Hi! I have a question about the ADC WD. I am trying to use it, being triggered by a touchscreen, I have set it as follow: static void MX_ADC1_Init(void){/* USER CODE BEGIN ADC1_Init 0 *//* USER CODE END ADC1_Init 0 */ADC_A...

Resolved! STM32 Black Pill not detected by ST-Link

I Recently bought a STM32F411CEU6 . It was working fine till i shorted two pins by mistake.The STM IDE says no target found when i try to upload the code .Only the power LED turns on but the USER LED doesn't.(The ST-Link still detects my Blue pill pr...

Resolved! id is not recognized , stm32f103c8

i have this problem https://community.st.com/t5/stm32-mcus-boards-and-hardware/error-in-initializing-st-link-device-reason-18-could-not-verify/td-p/314096 that ,  attach chip  photo  it doesn't look like a counterfeit chip   Open On-Chip Debugger 0....

stm32f103c8_no_id.jpeg

Resolved! STM32G0B1CET6N Eval Board.

Hello, We have been using this Processor for very long time in our 2 project stream.We are planning to use this part again, but for application suitability we need to verify this product as per our requirement.So, i wanted to ask is there any Evaluat...

Heena by Associate
  • 1234 Views
  • 2 replies
  • 0 kudos

Resolved! STLINK-V3 MINIE 3D Model

 I am wondering if ST could add a 3D model of the STLINK-V3 MINIE itself to the "CAD Resources". Currently, there are only STL files for ST's enclosure, but it would be helpful to have the 3D model of the PCBA itself to design other enclosures.

astep by Associate
  • 3111 Views
  • 7 replies
  • 4 kudos

Nucleo-64 3D printed base

I created this 3d printable base for the Nucleo-64 boards, to avoid damage to the bottom pin headers, reduce the risk of short circuits and as a convenient support during the prototyping and development process. I share it here hoping someone else wi...

Nucleo-64_Base.png