Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello, I've been trying everything for days to fix this error. They said to set the BOOT0 pin to GND. I followed these steps. I tried many solutions from YouTube videos and the STM32 website, as well as solutions from forums, but none of them worked....
Hi everyone,I am working on a project with the STM32H755ZI-Q (Nucleo H755ZI-Q) board, and I am following this tutorial for Inter-Processor Communication (IPC) using OpenAMP: Link to tutorial.The setup involves two processors (M4 and M7). Here's the ...
Hi all.I'm using STM32H747I-DISCO bord.According to user manual, Pin No.1 in Pmod™ is connected to PA11/PA0.And Pin No.1 in STMod+ is also connected to PA11/PA0.Then can I use PA11 as USART1_CTS via Pmod™ Pin No.1, and PA0 as GPIO via STMod+ Pin No....
I am trying to use the available example from software package - Microphone streaming. I Have installed audacity app, and follows the documentation related to X-NUCLEO-AMICAM1. LINK: UM2649 - Getting started with the X-NUCLEO-AMICAM1 analog MEMS micr...
I created a custom STM32 board for a motor controller, but I am having trouble even programming it using the STLink V2. I am using the STM32C071KBT6N MCU that I purchased from Mouser. I soldered it onto my board using drag soldering. I soldered other...
The power cable and the USB cable for kit interface are connected properly.When I connect the interface cable as per the the quick start guide, the LabTool does not recognize any port. If I go to settings - port: I can find no port to chooseIf I go t...
Where to download CAD ZIP files for STM32H753I-EVAL2 board and Nucleo-H753ZI board???I can't find ZIP files in https://www.st.com/en/evaluation-tools/nucleo-h753zi.html#cad-resourcesI can't find ZIP files in https://www.st.com/en/evaluation-tools/st...
Hi i want to enable Power module (Generally PWR EN) on which bus i can enable this bit in can of NUCLEO-H723ZGas for reference manual is used RM0468 Also if you find this please give me link to that data sheet and secion number as i can not find it i...
Is there a development board for specifically STM32F103C6T6A chip, (LQFP 48). I only see 64 pin version on this site. If there is no such board, what are my options? I specifically want to avoid using bootleg versions of the chip, so want to avoid us...
Hello everyone,I am working on a custom board using an STM32F103 (LQFP48) and connecting it via ST-LINK V2 using the SWD interface.However, when I try to connect, STM32CubeProgrammer reports:Error: No STM32 target found!The log shows that the ST-LINK...