STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F405 SWD and JTAG don't work

For some reason I am unable to connect to my custom STF32F405RGT6 board via SWD or JTAG.I originally had my board wired as this table below:ST-LINK/V2ST-LINK/V2My BoardMy BoardPin NumberConnector CN3MCU PinMCU Pin1Target VCC  2Target VCC VCC3TRST  4G...

Parker_0-1755188289359.png Parker_1-1755188359888.png Parker_3-1755188548492.png Parker_4-1755188601896.png
Parker by Associate II
  • 1789 Views
  • 8 replies
  • 0 kudos

Power leds are blinking

 Hi I don’t know the reason, but my board’s ld2 and ld8 leds are blinking, and the program says  No STLink detection, even if I connect it to the usb port, what can be its reason? How can I fix it?

IMG_7491.jpeg
MÖZDA.1 by Associate II
  • 832 Views
  • 6 replies
  • 0 kudos

STM32H755BIT3 Supply connection

你好 我正在与 STM32H755BIT3 一起做项目。我设计的电路板的现状是,用DC-DC 3.3V电源上电后,芯片很快发热严重,不出现短路就无法下载程序。我推测这是由于外围电路的设计。 有人可以帮忙找出问题所在吗? 提前感谢大家的任何提示。 Translation: Hello I am working on a project with the STM32H755BIT3.The current situation of the board I designed is that after...

LLionel by Associate
  • 1131 Views
  • 1 replies
  • 0 kudos