cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32H723 Stop mode high current 4mA !!

NMast.1
Associate II

Hi all,
I am using the Nucleo-H723ZG board and I'm testing the consumption in stop mode, running the example from the ST repository NUCLEO-H723ZG\Example_LL\PWR\PWR_EnterStopMode.
The code compiles without any warning and I use the stlink of the nucleo to program it.
I removed the Jumper JP4 (VDD_MCU) and in its place I inserted a precise ammeter (HP34401A)
The current measured at the moment of STOP is about 4mA!!
Can anyone help me?
Thanks a lot,
Nicola

1 ACCEPTED SOLUTION

Accepted Solutions

I found the solution...
Many thanks to everyone.

WhatsApp Image 2025-01-31 at 16.53.23.jpeg

 

 

View solution in original post

6 REPLIES 6
AScha.3
Super User

Hi,

so look at the circuit of the board to see, what still is connected - and check, that you switched it off.

https://www.st.com/resource/en/schematic_pack/mb1364-h723zg-e01_schematic.pdf

 

btw  4mA ...still driving a LED ? :)

 

If you feel a post has answered your question, please click "Accept as Solution".

Hi Asch.3,
thanks for the reply.
But when I measure the current instead of the JP4 jumper it is only that of the MCU without anything else.
The jumper is actually made to measure the current of the MCU.
Thanks,
Nicola

Andrew Neil
Super User

As @AScha.3 said, check that what you're measuring isn't including other things on the board - especially the ST-Link:

https://community.st.com/t5/stm32-mcus-embedded-software/how-to-check-stop-mode-current-consumption-on-nucleo-l073-board/m-p/763513/highlight/true#M59118

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

@NMast.1 wrote:

The jumper is actually made to measure the current of the MCU.


But that will include any current sourced from the MCU;  whether intentionally, or by "leakage" to other stuff on the board - such as the ST-Link.

See the link I posted earlier.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

I found the solution...
Many thanks to everyone.

WhatsApp Image 2025-01-31 at 16.53.23.jpeg

 

 

How to get a screenshot - rather than photographing the screen:

https://www.techrepublic.com/article/how-to-take-screenshots-in-windows-10/ 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.