Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Yesterday, while debugging in mBed, I experienced strange problems like being unable to debug, unless i unplug and replug the board. Maybe unrelated.Today, the board is not recognized (USB descriptor problem it seems).
MCU not getting selected. Referred tutorial given in STM website. Using STLink debugging configuration. Any extra jumper connection in board required ?? Please inform if any.Development Board - STM32 Discovery L475 MCU
Using ST-LINK we need to program a device but the data which needs to be programmed is highly sensitive so the CLI cannot be used. Are there any suggestions how to proceed with this programming other than writing our own functions? Are there any modu...
Hello, I tried STM32CubeIDE v 1.0.0 and 1.02 but I think the somethink important doesn't work with a STM32L422CB and maybe with more new MCU. It's old version of J-Link. I can not set new or oldest version J-link in debug configuration. And also ST-l...
Hi I am designing a PCB for sampling 4 audio channels from 4 I2S MEMs microphone and doing some audio processing on it. My MCU STM32F407 has 5 I2S peripherals and I plan to use I2S2 and I2S3 for each pair of microphones. The configuration of each I2S...
I'm attempting to program a Blue Pill board using the Arduino IDE and an FTDI232 board.I am using the STM Cores board library V1.7.0I receive an error: " STM32_Programmer_CLI.exe not found. "I downloaded the "en.stm32cubeprog.zip" However it looks...
Hi, i'm interesting in STLINK-V3MODS but i can't find any distributor on the web. Is this module available? Someon kwons if STLINK-V3MINI has the flat cable connector soldered?
Currently using STM32CubeIDE version 1.1.0Cannot see ULINKpro in the dropdown list within the debugger configuration tab.It has ST-LINK (ST-LINK GDB Server), Segger Jlink, ST-LINK (OpenOCD)uProcessor targeted is STM32F407
Where is a hardware design guide / minimal recommended connections for STM32H753VIT6?I am new to ST MCUs but ST's competitors generally have a chapter in the datasheet or an application note on this subject.Thank you
Hi,I just bought a stlinkv-3set programmer / debugger.I currently use Eclipse IDE together with texane / st-link and openocd.I've always worked with the discovery boards (F051 and F746G) without any problems. They use the stlinkV2 or V2.1 protocol an...