Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I am using Ubuntu 18.04 VirtualBox on MacOS with STM32G484QE-EVAL baord. While switching to STM32CubeIDE 1.1.0, the debug tool will ask to upgrade the STLINK V3 firmware. Clicking the upgrade button and "STLinkUpgrade 3.3.0" will start. Click "Open i...
Hi, every one, I am new in STM32. Recently, i got 2 STM32L4R9I - Disco. the first one work perfectly fine. as i plug the STLink to connect the first one to the Laptop. it works and the connection also appear on Device manager. i can load and debug th...
At time of debugging my application card based on stm32f072 controller I am getting Debug warning as verify error from address onwards 0x08003800 & and controller enters in hard fault. Current application code size is reach just around 20KB In case I...
I need to find some layout resources for the UFBGA-132 package for the STM32.Thanks
Hello,as the title tells, I would like to power up a Nucleo 144 board (STM32l496) from its User USB connector. I've read the documentation and it tells that it is not possible, but would it remain impossible even with an external regulator connected ...
STM32F030R8Blank project, no CMSIS, no Cube libraries.Code copied from my old TrueStudio project.I use old startup_stm32f030x8.s with some modifications.If I change startup vector table start entry to my function (named not Reset_Handler but Boot_Sta...
Hi everyone,I have to write a custom external loader and reviewed the examples. The read text of these examples say that after the folder placed inside cube files, it will run seamlessly. However, I can't do this, it needs lots of files to build. Ple...
Hi EveryoneI am trying to view variables in Keil MDK5 Logic Analyzer Window therefore I have enabled trace and do the required settings of my STM32F429I discovery board. But When I open Debug window and run my code I get trace: No Synchronization mes...
Does the STM32F0x1 line have SWO (the output trace) in its debug port?Reading the User Manual of STM32F0-Discovery (UM1525) it looks like SWO is on pin PB3.But the Reference Manual for the board's STM32F051 (RM0091) does not even mention SWO, only S...
Hello!I have designed a custom board, i have attached the schematic of it. My problem is that I have an ST-link v2 and i cant connect to it, i get target not found. Is my schematic correct or I have missed something? I have power and ground on all n...