Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi all,Is there any way to save SWO output to file using any official STM product?Best scenario would be to use st-link server.As we can have SWV it in STM32CubeIDE would be nice to have a option to save it to file.Regards,Pawel
Erase Done.Programming Done.Contents mismatch at: 08000360H (Flash=FFH Required=00H) !Contents mismatch at: 08000361H (Flash=FFH Required=20H) !Contents mismatch at: 08000362H (Flash=FFH Required=70H) !Contents mismatch at: 08000363H (Flash=FFH Requi...
I've just installed the latest version of STMCubeIDE on a Mac and am trying to flash a simple program generated by the IDE. I have installed the L4 pack.The firmware on the ST-LINK has been updated.I have no other ST boards and I am not sure if it i...
Hi everyone,I have a problem with the ST-Link V2-1 that are embedded on the nucleo boards. I use the ST-Link utility CLI as an external tool in Atollic TrueStudio to program my nucleo boards. However after the programming operation finishes, the CLI ...
My MCU is loaded with the test program at the supplier. But when I loaded the actual program, it did not allow me to erase or read the chip, and the device was protected.
Is there some software configuration to do this procedure?Thanks
Hey,I am using STM32F103RET6 MCU in my own project and program it via SWD through Nucleo F446RE's ST-Link. Since I activated CAN peripherial I can't load a project to the MCU. I don't know if CAN is the problem.When I try to load a program through ST...
Similar to I2C bus capacitance, I want to calculate individual pin driver and output capacitance.Is there any related documents for such?
The STLinkUpgrade tool does, but the programmer does not. I am using STM32CubeProgrammer V2.2.0 and it does not see STLink V3 devices running the Debug+2VCP+Bridge firmware.
Anybody else getting this issue?Upgraded from STM32CubeIDE 1.02 to 1.1. I imported my previous project. ST-Link debug/upload was non-functioning. I have since downgraded back to 1.0.2 and ST-Link debugging/upload is functional once again. I don't hav...