2019-07-27 8:32 AM
Hi,
I just bought a stlinkv-3set programmer / debugger.
I currently use Eclipse IDE together with texane / st-link and openocd.
I've always worked with the discovery boards (F051 and F746G) without any problems. They use the stlinkV2 or V2.1 protocol and the st-link utility works correctly.
When I plugged my first new programmer, STLINK-V3SET, the st-link utility still refuse to recognize it.
Launching the st-info utility simply I got the following:
Found 0 stlink programmers.
I've already put the appropriate file in /etc/udev/rules.d (filename: 49-stlinkv3.rules).
Issuing the lsusb -v command I get the following:
mmazza@linux9:~/ARMtoolchains/stlink-master/build/Release$ lsusb -v
Bus 005 Device 007: ID 0483:374f STMicroelectronics
Device Descriptor:
bLength 18
bDescriptorType 1
bcdUSB 2.00
bDeviceClass 239 Miscellaneous Device
bDeviceSubClass 2 ?
bDeviceProtocol 1 Interface Association
bMaxPacketSize0 64
idVendor 0x0483 STMicroelectronics
idProduct 0x374f
bcdDevice 1.00
iManufacturer 1 STMicroelectronics
iProduct 2 ST-LINK/V3
iSerial 3 005200363137510239383538
bNumConfigurations 1
<more>
Any ideas.
I'm really stuck.
Thanks in advance,
Max
2019-07-27 8:38 AM
Find one of the developers, send then a pod and PayPal them some cash?
2019-07-27 10:11 AM
For a programmer, have a look at https://github.com/UweBonnes/pystlink/tree/features. It know the V3.
2019-07-27 12:05 PM
@Uwe Bonnes Thank you! I will try it as soon as possible.
Max
2019-10-30 6:04 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.