Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I'm trying to get myself situated to program comfortably with my STM32 Blue Pill and STLink V2 USB interface. However, I've run into an issue when trying to gain access to the VCP (Virtual COM Port) that the STLink is supposed to open up for me when ...
Hello,Iam using STM32H743 Nucleo board.Suddenly The Red LED (Over current LED) is glowing in my Micro controller. I have cheked all the connections properly there is no short circuit in it. Because of this i cant able to load the Program in it It is ...
I can connect from STM32CubeProgrammer via ST-Link/v2 running V2J3457 when I lower the frequency from 9000Hz to 2250Hz. However, I can't connect from the STM32CubeIDE debug because there is no (obvious) way to set the frequency.
Starting ST-LINK_gdbserver with -the -s option, flash upload show success. However the "compare-section" command show mismatch"(gdb) compare-sectionSection .text, range 0x8000000 -- 0x8003420: MIS-MATCHED!Section .data, range 0x8003420 -- 0x80035bc: ...
I installed the driver for the ST-LINK V2 on Windows 10 (STSW-LINK009). The Installation was successful. Unfortunately the device can't connect to the USB port and is blinking red. I even can't find the driver in the Device Manager in Windows. The so...
I designed a board based on an STM32F303CC and I am unable to upload any code to it. I'm using STM32CubeIDE with an ST-Link/V2 programmer. I've connected Pin 7 to DIO and Pin 9 to CLK. The board uses USB for it's 5V power supply which is transformed ...
I'm writing some code for our product flash programming via ST-Link_CLI.exe, because there are two kinds of STM32 MCU in one boards, one is STM32F417 another is STM32F09, two ST-Link connected to one PC via USB port. I would like to send command to g...
Here is what I did - From CubeMX, I mistakenly change port configuration of port pin PA14 from SYS_JTCK-SWCLK to GPIO_Output.Apparently this disabled the debug / programming channel of the target micro controller on the board.Later I reset the port p...
I am using STM32F107RC MCU. And programming it using ST LINK utility in SWD mode.By mistake I have set the READ Protection & WRITE protection in its Option Bytes.Due to which now my controller is locked and I am unable to erase or reprogram it.Enclos...