Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi everyone,I'm currently working on a project where I need to establish UART communication between an STM32L053R8T6 Nucleo board and a Chafon RFID reader IC. The goal is to send commands from the STM32 to the reader and receive tag data in response....
can some one please tell me why is the schematics the pd8 is connected to gnd?here is a picture of the schematics
Table 20, "CN9 ZIO Connector pinout" on page 40 of "UM2407 User manual Rev 2 - STM32H Nucleo-144 boards (MB1364)" lists the wrong pin name for pin CN9-15. It is listing PE0 while it should be listing PE9.
I'm attempting to erase & program a STM32H7x using a STLink V3Mods and OpenOCD (a recent official release).It fails with a "read version fails".When i try using a STLink V2 (host, openocd script and target device unchanged), it works just fine.I've s...
Hello ST, Can you confirm if the hardware of the https://www.st.com/en/evaluation-tools/steval-66gymai.html#overview is compatible with the https://www.st.com/en/evaluation-tools/stm32n6570-dk.html. Can i connect them together with the FCC cable (MIP...
:wrench: STM32 Samples: A Developer’s Time SinkI’m not a novice in software at all — and this isn’t just about one sample. It’s about STM’s consistent failure to respect developer time across their software stack especially modules of other vendors ...
I have a Nucleo-64 STM32F411RE. It's cool. I can program it, debug code and everything nice. But it's too large, however! I need to pack my projects to be as small as possible in order to ship to the market. I need an official stm32 board with an in...
Hello,I'm working with B-WL5M-SUBG1 hardware for experiencing STM32WL5MOCH6U. I ran the application from Repository\STM32Cube_FW_WL_V1.3.1\Projects\B-WL5M-SUBG1\Applications\SigfoxI got current of about 2.3mA in standby mode instead of less than 1uA...
Hi, I have a STM32N6570-DK and I see that the available demo code is up to v1.3.0How do I determine what version of code was shipped on the DK?Is there a document that details how to upgrade the code if it’s needed?STM32N6-OOBSTM32N6570-DK Out-of-the...
Hello everybody,I have a question related to the STM32N6570-DK eval kit. Is it possible to change the position of the BOOT switches when the board is powered by USB-C ST-Link ? Or do I always have to power-off the board ?Thanks Max