2025-03-14 5:08 AM - last edited on 2025-03-14 6:21 AM by Andrew Neil
I built and debugged the default example UART_HyperTerminal_IT using the STM32N6570-DK board, but the following error occurred. How can I resolve this issue? I am using the latest versions of ST-Link and all related software.
STMicroelectronics ST-LINK GDB server. Version 7.10.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
2025-03-14 5:28 AM
Hello @wwnsok2
Do you changed STM32N6570-DK in DEV_BOOT mode to be able to debug it?
Check UM3300 section 7.7 Boot options
https://www.st.com/resource/en/user_manual/um3300-discovery-kit-with-stm32n657x0-mcu-stmicroelectronics.pdf
You can also you refer to this post:
Best regards,
Romain,
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-14 6:12 AM
2025-03-14 6:29 AM
@wwnsok2, the capture you shared doesn't help.
Can you confirm you configured BOOT0 and BOOT1 switch on STM32N6570-DK as the picture bellow:
Then, press one time on NRST black button, LED2 Red must be ON and it confirms that STM32N6 is in DEV_BOOT mode. After that you can start a debug session.
Best regards,
Romain,
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-14 10:35 AM