STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Where can I buy ST Link V3 mini cables?

ST link V3 Mini uses dense 10 lead cables. Ebay doesn't find anything suitable and Digikey has some I think, but it is expensive to order just some cable.This I think is one https://www.digikey.fi/product-detail/en/adafruit-industries-llc/1675/1528-2...

LMI2 by Lead
  • 2517 Views
  • 4 replies
  • 0 kudos

help - stlink can not connect to target

ive been trying to get my first board with a stm32 running. Im using an stm32f031k6 and an STlink v2 and I keep on getting the "can not connect to target" error. It seems like I can connect through the stlink utility to the programmer, and I've check...

deep_rune by Associate III
  • 2327 Views
  • 4 replies
  • 0 kudos

writing into EEPROM failed in Second attempt

Hi, i am using st link v3. with stm32 cube programmer v2.4.0.hardware = stm32L071set the RDP level to AA.i can write the eeprom only once on same address, if i try to change the value on same address then cube programmer is block. please take look on...

0693W000001rqsZQAQ.png 0693W000001rvF8QAI.gif
Jutt by Associate II
  • 1774 Views
  • 2 replies
  • 0 kudos

Resolved! Windows command line tool for SWD viewing

Stupid newbie question: apologies if I've missed this but I'm looking for a Windows command-line tool to capture SWO output from the target, i.e one that connects to the target, sets the appropriate register bits to configure SWO output etc., takes a...