STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H7A3 unusable for VGA

Getting stable V-sync and H-sync pulses is critical for clean VGA output. Getting these completely stable on the H743 was difficult and required multiple iterations of different PLL settings. but was possible.On the Nucleo-H7A3ZIQ it has proved compl...

PMath.4 by Senior III
  • 3360 Views
  • 9 replies
  • 0 kudos

STLINK Problem , (possibly p-nucleo bricked ?)

HiThis is the first time I`m using STM32 tools and probably made a mistake hence I can`t connect to Nucleo 68 board.When I try to connect using STLink Utility I receive22:31:40 : Can not connect to target!         Please select "Connect Under Reset" ...

TGUCL.1 by Associate III
  • 1708 Views
  • 5 replies
  • 0 kudos

Why can't I connect the ST-Link/V2 to my target board when the target is self-powered? (using the SWD)

If my board is not powered and the power is provided by the ST-Link, then I can program/erase all the time without issue. However for debugging it is not useful. As soon as I connect the power to the target I loose the connection.Few thingsSWDCLK and...

MCons.2 by Associate II
  • 1268 Views
  • 1 replies
  • 0 kudos

Wifi Chip is not properly soldered hence came out when the board got delivered. How to fix it ?

Inventek systems ef-wifi module got detached from the board. Hope this is the wifi module. But How can I attach it back to the board. If thats not possible can I get a new replacement the board and how long would that take ? Since its a brand new boa...

DRAME.1 by Associate II
  • 2297 Views
  • 6 replies
  • 0 kudos

STLINK Cannot Detect Target Voltage

I am using an STLINK V3SET and the STLink Utility v4.5.0.0. I have opened up the V3SET and I am measuring at the pins of the connector to the target the correct 3.3V between pins 3 and 5 as indicated in the user manual. This voltage is coming from th...

WTetl.1 by Associate
  • 1422 Views
  • 1 replies
  • 0 kudos