Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
In the picture:pin 1 top left: VDD 3.3V 4 100n to GRND 14 to GRND 15 to VDD 16 to GRNDon their left 1µ and 10n F decoupling VDDA VSSApin 32 top right : VSS 0V GRNDpin 31 10K ohm to GRND 24 SWD clk 23 SWD dio 17 to GRN...
Hello STM enthusiasts,I am reaching out as I am having a puzzling issue with connecting to my STM32 chip with an ST-LINK V2.What I have for a set up is:OS: Windows 10 x64 bitIDE: Atollic TrueStudio v9.1.0Debugger/Programmer: ST-LINK V2Chip: STM32F030...
Can anyone please let me know, how is this possible?
I have got a custom PCB using STM32F4. I don't have any capacitor connected to the VCAP Pin and I wonder if this is necessary or not. Which is the use of VCAP and do I need to add it to my design? What can I do to solve my problem of no having one if...
For a long time I have been using the following setup:two STM32H7 eval boardsone gdbserver session for each STM32, with a different portremote debugging on the two STM32I just switched from STM32CubeIDE 1.0 to 1.10.1 and now I have this weird behavio...
I have two devices I am looking to integrate with STM32 MCPUs. One is a Honeywell HG1125 IMU and the other is an WFF93 Encoder.Both devices use LVDS signalling. I don't know much about that signaling at this point, but I am taking a broad stroke fi...
I see from the schematics in datasheet UM1956 that there is a reserved CN2 connector with SWDIO and SWCLK, NRST can be found on CN3. But I do not see any jumpers to switch whether ST-LINK is used to program on-board Nucleo MCU or an external MCU like...
HelloI may have misunderstood:By cutting some SBs offand soldering on CN2 the embedded STLinkv3 can be used externally ? meaning on other targets/boards ?
I've gone over the hardware with a multimeter and all the pins have the right continuity, I've checked the design against the Nucleo-144 L552ZET6Q schematic and it checks out so far, and I've also checked the connections to the ST-LINK/V3 pins I'm us...