Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello-We are working with two different boards for the STM32L062, schematics of which I have attached. The first is a bare-bones development board for general testing and the second is our product. I have a Cube32MX project that enables the feature...
Hi,I use ST-Link V2 and CubeProgrammer_CLI.exe for programming STM32. Unfortunatelly sometimes during programming the connection between MCU and ST-Link is lost. If this happen there is a high probability the ST-Link stays in some weird stuck state a...
In other words, is the Zio a subset of the Morpho?
Hello,I am working STM32H745 controller. I am trying to connect STLINK_V3 SET to my customboard. But I getting the errors I am attaching the images ,I set the Debug as serial wire and device is in Connect Under Reset. What things I have to check, als...
Working on interfacing with the evaluation board however I don't know where any I/O is mapped.For example CN9 PC0 what gpio is this mapped to ? What I have done with other MCUs is reference the evaluation board schematic to know the corresponding pi...
I have the STM32L451RET6 and i would like to integrate it to my PCB. This PCB is directly connected to a PC over USB. So to communicate with the STM32 i need a FT231XS-R. So i am not sure how the schematic looks like.
Hi all,I'm using STM32F767 Microcontroller.For flashing FW to the controller I'm using STM32CubeProgrammer through USB DFU mode.By making the BOOT pin high, I tried to connect the device with programmer through USB.Then I observed the error screen po...