cancel
Showing results for 
Search instead for 
Did you mean: 

What is the peripheral (circuit label ) diagram of STM32L476RGT6U?

Prajnyajit
Associate II

I'm working with STM Nucleo-L476. I want to mount the IC STM32L476RGT6U on my PCB. I got the footprint successfully; however, I'm unable to find the peripheral connection of the particular IC. I got the pin diagram clearly and know exactly where my sensor pins should be connected but what about circuit label peripheral means where R, C, L, crystal oscillator should be connected? I did not find any material related to this. Please help and provide a peripheral connection diagram.

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Prajnyajit
Associate II

It is an LQFP-64 packaging.

TDK
Super User

Pinout information is in the datasheet.

https://www.st.com/resource/en/datasheet/stm32l476je.pdf

See also AN4555: Getting started with STM32L4 Series and STM32L4+ Series hardware development:

https://www.st.com/resource/en/application_note/dm00125306-getting-started-with-stm32l4-series-and-stm32l4-series-hardware-development-stmicroelectronics.pdf

CubeMX is a good resource for doing pinout allocation.

If you feel a post has answered your question, please click "Accept as Solution".

Please let me know, where is the peripheral circuit diagram. I have seen these materials but where is the exact board-level diagram?

Board schematics are available under CAD Resources on the product page.
If that’s not it, not sure what you’re looking for. You linked a chip, not a board. All the peripheral pin linkages are in the datasheet.
If you feel a post has answered your question, please click "Accept as Solution".

If I refer the Figure 14. Reference design STM32L4 Series / STM32L4+ Series (from AN4555) for the connection of PCB with peripheral, will it be ok? Just want to verify?