Skip to main content
BTrem.1
Senior
September 11, 2021
Solved

On STM32G431 is the BOOT0 pin (PB8) no pull-ups or weak pullup?

  • September 11, 2021
  • 3 replies
  • 3205 views

On the STM32G431x6/x8/xB UFQFPN48 I've been assuming that BOOT0 pin PB8 was a weak pull-up during reset, but in trying to track this I think it has no pull-ups/ pull-downs. Is this the case?

This topic has been closed for replies.
Best answer by TDK

You can use the nBOOT0 option byte to override the value on the pin. Otherwise, you need to ensure it's low or high, depending on your intention.

It should be low if you want to run user code. Whether you do that with a pulldown resistor or an FPGA pin is fine. However, you need to ensure it's low when the STM32 is booting up. The best way to ensure this is an external resistor on the line.

Pulling it up will run the bootloader on startup, rather than user code.

Leaving it floating leads to undefined behavior (unless overridden with option byte mentioned above).

3 replies

Tesla DeLorean
Guru
September 11, 2021

Floats, if you use it for BOOT0, pull it low externally to ensure reliable operation. Only the JTAG/SWD pins have pull up/down at power on

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
BTrem.1
BTrem.1Author
Senior
September 12, 2021

Presently we use an FPGA open drain output to pull it low. It does not need a pull-up? A float is okay? Thanks!

TDK
TDKBest answer
September 12, 2021

You can use the nBOOT0 option byte to override the value on the pin. Otherwise, you need to ensure it's low or high, depending on your intention.

It should be low if you want to run user code. Whether you do that with a pulldown resistor or an FPGA pin is fine. However, you need to ensure it's low when the STM32 is booting up. The best way to ensure this is an external resistor on the line.

Pulling it up will run the bootloader on startup, rather than user code.

Leaving it floating leads to undefined behavior (unless overridden with option byte mentioned above).

"If you feel a post has answered your question, please click ""Accept as Solution""."