STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Nucleo-h563zi factory onboard example applicatio

I'm experimenting with the nucleo-h563zi board again using the examples in CubeIDE and CubeMX but I would like to end up replacing the LED/UserButton application that was originally installed when I received the board.  Can't find it.  Can someone po...

TJM by Senior II
  • 2714 Views
  • 2 replies
  • 1 kudos

CCA02M2 Quick Start Mics not Recognized

Hello I am working on a group project in which we have a Nucleo-H723ZG and a CCA02M2 expansion board. We attempted to follow this quick start guide: https://www.st.com/resource/en/product_presentation/x-nucleo-cca02m2_quick_start_guide.pdf  However, ...

slrobers by Associate
  • 1305 Views
  • 1 replies
  • 0 kudos

Resolved! 90 Degree Phase Shift

Hii, i am new at stm32 controller & i want a pwm phase shift of 90 degree . So can anyone plz tell me that how i will generate the phase shifted pwm (what parameters we need to set to get it)

Harsh_18 by Associate III
  • 2722 Views
  • 2 replies
  • 2 kudos

STM32f207's MII with Marvel's MII

Hi All,     I'm developing a project, in which I've connected the MII port of STM32F207 with Marvel IC 88E6060 (Ethernet + fiber switch) MII port 5 but the firmware support (SPL for STM32F2XX) provides libraries for DP83848 PHY only.      Hence, if I...

J-Link and NUCLEO-U5A5ZJ-Q or STM32U5A9J-DK

Does these boards work out of the box with an external debugger like a J-Link Ultra+?  I see they both support a MIPI10 connector (and one supports a tag connector as well) that leads me to believe it supports an external debugger.  However, I can't ...

boxtor by Associate II
  • 1780 Views
  • 2 replies
  • 0 kudos

Resolved! Help Configuring I2S with H723ZG with CCA02M2

Hello,I am using a H723ZG Nucleo 144 STM32 Board, with an CCA02M2 expansion mems mic board attached. I am wanting to read in audio data from the 2 built in mics on the expansion board using I2S with the nucleo board.  I am unsure how to setup/configu...

slrobers by Associate
  • 2867 Views
  • 4 replies
  • 0 kudos