STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Stm32F4 CANbus Acknowledgment error problem

Hello everyone. The last time I opened a form related to bit timing, I realized that the problem was in the Canbus transceiver. I added 1-2 revisions and replaced it with the MCP2551 transceiver. Even though there is a device on the other side, I get...

Sergen by Associate III
  • 12634 Views
  • 12 replies
  • 4 kudos

Resolved! No examples for Nucleo-H743ZI2 in STM32CubeIDE but Nucleo-H743ZI examples marked as obsolete?

Hello,I have the new Nucleo-H743ZI2 board (note the "2" at the end of the board identifier).  I was trying to import some example project for the board using STM32CubeIDE example selector.  However I am stuck.  Completely.  The only examples availabl...

bczwartk by Associate II
  • 5021 Views
  • 7 replies
  • 3 kudos

Resolved! Virtual COM Port for NUCLEO-F070RB not working on Windows 11 - Regs

Dear ST community,                                 I am facing an issue with the virtual COM port for my NUCLEO-F070RB board. It is not working on my Windows 11 computer, and I am not sure how to resolve this. Can you please provide me with some guid...

SANTHOSH1 by Associate II
  • 3249 Views
  • 6 replies
  • 1 kudos

Resolved! STLINK-V3PWR hardware failure

I'm using my V3PWR probe for weeks now... but this morning it refuses to work. It was working yesterday evening with the same setup.When I connect to the USB-C cable, no led at all , no USB enumeration ... nothing !! I changed the cable without succe...

PJEN by Senior
  • 3233 Views
  • 5 replies
  • 0 kudos

Stm32f7 ad Marvell switch over mii

Hi all,We need to interface a stm32f7xx with marvel switch over mii connection to port 0. If you have any example of interfacing such switch please share. Normal stm32 network example show only assigning ip address to phy. How do we handle switch? In...

Ashi by Associate II
  • 1580 Views
  • 1 replies
  • 0 kudos