Hi Thomas,Greetings.Could you kindly clarify on the following point:If we are going with single SPI interface, whether we need to use pull-up resistors for HOLD (Pin#7) and W (Write Protect, Pin#3) pins as it is mentioned in the datasheet of M95P32-I...
Hi Thomas,Thank you for the response.As of now we are going with single SPI. But we will consider the recommendation of choosing Quad SPI and shall revert back if I have further queries.Thank you once again for your tremendous support. Best Regards,S...
Hi Thomas,Hope you are doing great.In our project we will be using Single/Dual SPI and not Quad SPI.Could you please provide reference schematics on Single/ Dual SPI of M95P32-I interfacing with STM32U585ZIT6?Best Regards,Sreejith