2023-04-06 7:55 AM
2023-04-07 2:43 AM
Hello @Tajwar.Chandel ,
Did you try with STM32Cubeprogrammer?
Try changing the USB cables.
Check the jumpers configuration following this UM2189.
Try connecting with mode 'under reset'.
Imen
2023-04-07 3:09 AM
Hi Imen,
Thanks for the reply. I have tried after replace the micro USB cable. But still failed. I have traying to connect with STlink-V3Set. Result target no device found. When i connect the same target with Nucleo ST link then its connected. Why ? I just want to know why its is not connected with STLINK-V3SET debugger.
If our hardware was faulty then the device could not connect with Nucleo-ST link.
Kindly respond.
Regards,
Tajwar
Mob. +91 9857325411
2023-04-07 5:21 AM
Show how physically connected.