STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! After installing the program with ST-LINK, when I turn off the power and return it, the last program I installed does not work.

Hi. I am using stm32L010C6Tx. After installing the program with ST-LINK, when I turn off the power and return it, the last program I installed does not work. I need to reload the code. I wondered if it wasn't writing to your Flash, but it looks full ...

ZKURT.1 by Senior
  • 3098 Views
  • 6 replies
  • 0 kudos

Resolved! Compatible Displays (LCD)

Hi there, Just wondering if there are any 3.5" - 5" displays that are compatible with the Nucleo-H755ZI-Q. I require a standalone screen that is not attached to a development board. I am currently using the below screen: https://www.dfrobot.com/produ...

isaacjack by Associate II
  • 2958 Views
  • 3 replies
  • 2 kudos

Resolved! stm32f767zi nucelo ethernet hardware setup : Can we use our laptop as a router for testing?

Hello  everyone,It is a quite basic question, I have this stm32767zi nucleo board with a LAN driver and rj45 connector, and I intend to test the basic ping/web server examples.So for now, I do not have a router with me, so I was wondering, if I could...

Anare.1 by Associate III
  • 7414 Views
  • 10 replies
  • 6 kudos

ST-Link cannot more flash external Target

Hello,Situation: I have a Nucleo WB55 board that is able to flash the internal SMT32 micro with the embedded ST-Link.I want to use this Nucleo to flash a custom board with the embbedded ST-LINK, disconnecting the jumpers and connecting the lines prop...

MFail.11 by Associate III
  • 3648 Views
  • 7 replies
  • 0 kudos

Resolved! Production flash tool for dual core STM32H745

I am releasing my first product using a dual core STM32H745.  Our board manufacturer is using Segger J-Flash to load our application hex files.  The process for flashing our released firmware is to load a Segger project setup for the M4 core and our ...

GHolc.1 by Associate III
  • 7025 Views
  • 5 replies
  • 4 kudos