User Activity

Hello all,I have been trying to implement the MSC_Standalone example (device mode with SD card) with the STM32469 discovery board and CubeMX for some time now (OTG_FS_MODE).The example works perfectly in standalone mode, but when I now try to set up ...
Hi all,is it possible to write a bootloader which sits at the beginning of the CM4 memory block and updates the CM7 as well as the CM4 (userapp sits in the memory area of the CM4 behind the bootloader)?I imagine it like this: The configuration bit th...
Hello all,this is my first post in this forum.I am in the process of developing my own bootloader for a firmware upgrade via SD card with the Eval board STMH757I.So far so good, with the help of the FirmwareUpgradeStandalone example, I was able to ge...
Kudos from