STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UCPD pin protection

The UCPD / CC circuit is one of the few that connect an MCU pin to the PCB connector. There does not appear to be any specific information on how to protect this pin. Thus, I assume the same rules as other pins apply. That means 5V  or even 3V being ...

Carl_G by Senior III
  • 286 Views
  • 4 replies
  • 0 kudos

Resolved! STLink not appearing in Device Manager

I installed stsw-link009 on my pc so I could use the STLinkv3. The PC did not see the STLink-v3. I then installed STM32Cubeprogrammer thinking that would fix the stlink driver issue but when I look under devices USB in the device manager I can not se...

Kat1234 by Associate II
  • 466 Views
  • 5 replies
  • 1 kudos

Dual SDRAM interface

Hi everyone, I'm designing a board with an STM32H7[STM32H757XI] and two MT48LC16M8A2P SDRAM chips to get 16MB (16-bit wide). I'd appreciate a schematic review before PCB fabrication. Hardware:- MCU: STM32H757XI- SDRAM: 2x Micron MT48LC16M8A2P (4Mx8, ...

hao033 by Associate II
  • 289 Views
  • 2 replies
  • 0 kudos