2025-03-17 9:26 AM
Hi,
I am using the STM32L4 B-L475E-IOT01A board with Wi-Fi module Inventek system ISM43362-M3G-L44.
I have seen the example WiFi projects but they do not have the .ioc file. So my question is, is there any middleware available in STM32CubeMX which can help me implement WiFi connectivity via USART?
The communication interface between the stm32 board and the WiFi module is SPI3 by default but the documentation says that use of USART3 is also possible, and USART3 is what I want to use.
So any easy ways to do that? Any available middleware in CubeMX? Or is any example project available online?
Thanks!
Solved! Go to Solution.
2025-03-18 1:42 AM - edited 2025-03-18 2:04 AM
@fa31 wrote:I have seen the example WiFi projects but they do not have the .ioc file. !
Indeed - not all projects have .ioc files:
On the Inventek ISM43362 WiFi module, and ST examples:
2025-03-17 2:45 PM
Here you can find help and advise for your project:
2025-03-18 1:42 AM - edited 2025-03-18 2:04 AM
@fa31 wrote:I have seen the example WiFi projects but they do not have the .ioc file. !
Indeed - not all projects have .ioc files:
On the Inventek ISM43362 WiFi module, and ST examples:
2025-03-18 7:03 AM - edited 2025-03-18 7:06 AM
The https://github.com/nano256/ISM43362-M3G-L44-Driver repo that was mentioned in one of your links, worked for me.
Thanks!
If anyone wants to know how:
I copied the wifi.c and wifi.h files, commented out the "#include "helper_functions.h"" line from wifi.c file and modified my main.c. Then I stepped into the code and added "wifiRxBuffer" variable into watch and saw that it was getting response from the WiFi-module.
CubeMX modifications: I matched the cubemx configurations of the project with mine. Enabled SPI3 with the same settings, added GPIOs with same labels.
2025-03-18 10:14 AM
Continues - changing from SPI to UART:
2025-06-16 6:14 PM
Hi can you please tell me which pins did you use and what did you put in your main.c
Thank you!
2025-06-17 4:42 AM
Hi,
I used SPI3 to talk to the WiFi module. I used PC10, PC11 and PC12 pins:
My WiFi related main code is:
#include "main.h"
#include "b_l475e_iot01a2.h"
WIFI_HandleTypeDef hwifi;
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_DFSDM1_Init();
MX_I2C2_Init();
MX_QUADSPI_Init();
MX_USB_OTG_FS_PCD_Init();
BSP_COM_Init(COM1); // Enable UART for logging
BSP_SPI3_Init(); // Initialize SPI
wifi_configs(&hwifi); // Configure WiFi
wifi_join_network(&hwifi); // Join WiFi network
while (1)
{
// application
}
}2026-02-27 3:10 AM
Hi, I am also trying to use the inventek wifi module on this board.
What did you mean by this please: "Then I stepped into the code and added "wifiRxBuffer" variable into watch and saw that it was getting response from the WiFi-module."
Which code did you add this to?
And did you only use the wifi.h and wifi.c files form the repository in your project?
Thanks
2026-02-27 3:26 AM
@Playman wrote:What did you mean by this please: "Then I stepped into the code and added "wifiRxBuffer" variable into watch and saw that it was getting response from the WiFi-module."
That's single-stepping the code in the debugger, and using the debugger's 'Watch' feature to see the run-time value of that variable.
If you don't know how to use these debugger facilities, you should probably spend some time getting to know them before jumping into an advanced project like this.
eg, see here.
ST also have documents & videos on using the STM32CubeIDE debugger.
2026-02-27 4:15 AM
Okay, I will. Thanks