Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hi. I'm new to stm32 and have an h7 nucleo board to play with. This is my goal/problem.I want to read from the adc at reasonably high speed (2 Msamples/s, 10-bit will do as I don't need especially high resolution) for say 10 us. In that period I want...
Hello,I am using the P-L496AG-CELL02 board and am creating a program to read the value of ADC1 at pin PC_4. I want the VREF to be 3.3 V and not the internal 2.5 V. I have inserted the necessary solder bridge at R18. However, I get an error when initi...
Hello team,I am trying to integrate the STM32WB55RG board with a sensor. To validate the sensor data I need the USART peripheral. The USART is working when I try to implement the example code given. But the USART is not working when I try to use it i...
Hi I am designing a PCB using STM32H563ZI. Can you share the project files for NUCLEO-H563ZI ? I am using Altium Designer. If the files are in different format, I can import them to Altium. I have shared the link and the name of the evaluation board ...
Hello community,I wanted to know how can I check the compatibility of of QSPI NOR FLASH with micro-controller, what are the parameter that will affect selection.Are Infineon chips supported by STM32H7 family especially S25FL128SAGNFM003.
Hello AllCurrent Device setup:-NUCLEO-G071RB Eval boardSTM32CubeMX settings please find the attached screenshots.I'm trying to generate PWM signal using [ TIM3 channel 3] in NUCLEO-G071RB Eval board.Time period is 28 microseconds and width are 3 micr...
Hi, I have an STM32H563ZIT6 board and a simple task: to toggle the GPIO at maximum speed. I set the PA11 pin as an output pin and generated the code. Then, I used the HAL Library function [HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_11);] to toggle the PA11...
Hello, I am using a Nucleo 144 F767zi Board. I am try to get any command on the Virt COM Console. But I failed always. I tried very lot things from on youtube, on the Forum ... but I always failed.I see in the documentation um1974-stm32-nucleo144-bo...
Hello I have been trying to test the QSPI flash on the STM32H747, Based on the BSP test code. clock speed - 66Mhz prescaler-3Write operation Data size (KB) 1 4 10 50 75 100 Time taken(us) 618 2406 5337 16956 24233 31427 Read operation Data size (KB)...
I am running FREERTOS on both M7 and M4 on STM32H745 MCU. In general M7 gets booted up and release HSEM for M4 then it will start.Now my question , if there no activity in M7 (idle mode), would like to keep M4 actively running and put M7 in sleep. I...