STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

B-U585-IOT02A inport BSP project

Hello forum,Im trying to build a function based on the BSP example and all the peripheral sensors,when opening a new project and adding the libraries and drivers from the BSP example, nothing works.some of the files have missing defines which suppose...

Resolved! Can protocol baud rate configuration issue

Hi all  i use the stm32H735IGKx demo board,and would like to configure the can speed 500k. Below is my configuration:but i can't get the can data from the third party software at 500Kbpsand when i use the oscilloscope, i have to configure 800Kbps tha...

yuhui_0-1717639425662.png yuhui_1-1717639557203.png yuhui_2-1717639773552.png yuhui_0-1717642163953.png
yuhui by Associate II
  • 1530 Views
  • 1 replies
  • 0 kudos

Resolved! ST-LINK V2 COM Port

Hi, I have an issue with CubeIDE and ST-LINK.I'm trying USART communication with STM32F0F4, I write code and debug but I don't get COM Port. In device manager there is no port showing. I installed st-link009.In CubeIDE, i tried both St-Link GDB Serve...

0693W00000Su1Q4QAJ.png 0693W00000Su1QJQAZ.png
lre.1 by Associate II
  • 4555 Views
  • 4 replies
  • 2 kudos

Resolved! NUCLEO-H503RB Debugging Issues

So as these things go I have an, two actually, ST NUCLEO-H503RB dev board that I cannot get the debugger to work with it.  My colleague on the other side of the country has the same boards and a similar setup and he is having no problems debugging.  ...

JChrist_0-1717969403672.png
J.Christ by Associate III
  • 2970 Views
  • 5 replies
  • 2 kudos

Nucleo H723ZG docking options

Hello,I want to use the Nucleo H723ZG for a project with analog & digital lines and can't find the article number of the headers CN7, CN8, CN9, CN10. Is there a specific cable/contact type I can use to plug in the black header body? Or are the header...

Lysandros by Associate II
  • 1810 Views
  • 2 replies
  • 0 kudos