STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! NUCLEO-N657X0-Q User Manual

Is the a User Manual available for the Nucleo-N657X0-Q that contains the connector pinouts and jumper settings etc. The document (UM1727) listed on the documentation page https://www.st.com/en/evaluation-tools/nucleo-n657x0-q.html#documentation point...

theRat by Associate II
  • 3118 Views
  • 4 replies
  • 6 kudos

Debugging NUCLEO-H723ZG

Does any one know if this board can be debugged via the USB port that is connected to the PC or does one require an external debugging link?If external is required which one would you guys recommend I do have ST-LINK V2 which I use for smaller boards...

erastusC by Associate III
  • 3038 Views
  • 7 replies
  • 2 kudos

ST-LINK V3 is not working

Hello, I have two STLINK-V3 programming devices. But I can't program or debug. When I try to connect to my device with STM32CubeProgrammer, I get the errors "Unable to get core ID" and "No STM32 target found! If your product embeds Debug Authenticati...

MTURAN by Associate
  • 3442 Views
  • 5 replies
  • 2 kudos

Low consumption NucleoL476RG

Hello community, I have been working with the nucleol476rg in low power modes, but I have had some doubts during the tests I have performed, specifically using the stand by mode, I understand that only the RTC is active in fact with it I set the alar...

CamiloRJ9 by Associate II
  • 1508 Views
  • 3 replies
  • 2 kudos

ADC DMA stm32f401

Can the ADC write to the buffer faster than the buffer values are sent to PC?- Single channel ADC using DMA, non-circular, EOC every conversion- ADC is in 12-bit resolution but as I understand it writes a full 16-bits each conversion - Buffer size 10...