Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

New STM32 VSCode extension V2.0.0 released

Changelog Version 2.0.0 V2.0.0 implies a breaking change: CMake project generation has been moved from VS Code to STM32CubeMX v6.11.0 (and later). VS Code solution no longer has dependency on STM32CubeIDE (.cproject-files)VS Code solution no longer r...

VSCode How to install VCPKG on VSCode with Zscaler/Proxy

Issue:  The VSCode don't have the ability to route the extension network requests to the proxy (only VSCode application network is routed to the proxy) I -  the clean way (applies to network with Zscaler installed) ask for a Zscaler power user profil...

NawresGHARBI_1-1704443433898.png NawresGHARBI_2-1704443503313.png NawresGHARBI_3-1704443553581.png NawresGHARBI_4-1704443616206.png

Stm32f407 - Error "can't reset the core" with ST-Link.

Hello, I am using STM32f407IGT6 with Keil uvision and HAL library. When I try to connect the device with ST-Link and flash the software using the JTAG interface, I always see "can't reset the core" as the error.BOOT0 - Connected to GNDBOOT1 - Connect...

ajain20_0-1705490340060.png
ajain20 by Associate
  • 158 Views
  • 0 replies
  • 0 kudos

Log Data externally with STM32F767ZI and Simulink

Hey everyone,I want to use a STM32F767ZI to develop driving safety functions for electric scooters.The functions and Code are developed on Simulink using the Support Package for nucleo boards. I would like to log data from the MCU directly to a SD-Ca...

LKlau.1 by Associate
  • 497 Views
  • 3 replies
  • 1 kudos

Resolved! STSW-EDUKIT: How can I view the sprintf messages.

Hi Folks,Managed to get the source compiled and loaded for the inverted pendulum project.  Rather impressive.In the source code there's sprintf statements to inform the user on what's going on.My question is: How can I view these messages?I'm a bit r...

JMazu.1 by Associate III
  • 1096 Views
  • 13 replies
  • 0 kudos