Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

New STM32 VSCode extension V2.0.0 released

Changelog Version 2.0.0 V2.0.0 implies a breaking change: CMake project generation has been moved from VS Code to STM32CubeMX v6.11.0 (and later). VS Code solution no longer has dependency on STM32CubeIDE (.cproject-files)VS Code solution no longer r...

VSCode How to install VCPKG on VSCode with Zscaler/Proxy

Issue:  The VSCode don't have the ability to route the extension network requests to the proxy (only VSCode application network is routed to the proxy) I -  the clean way (applies to network with Zscaler installed) ask for a Zscaler power user profil...

NawresGHARBI_1-1704443433898.png NawresGHARBI_2-1704443503313.png NawresGHARBI_3-1704443553581.png NawresGHARBI_4-1704443616206.png

Cube Mx and Keil Cannot read project error.

Posted on November 13, 2017 at 15:56I created project in cubemx and opened in keil but i changed my computer and installed new keil,  i couldn't open projects  cubemx built. I don't know what is the problem ? I took some screen shots about my proble...

Value of ''__initial_sp''

Posted on December 11, 2017 at 13:30Hello , I am new to ARM cortex M processors and while doing some coding on my board using KEIL  i found thatat location 0x0000_0000 my debugger shows the value '0x2000_0660' . Thats the value of the MSP loaded. bu...

n.serina by Associate III
  • 263 Views
  • 1 replies
  • 0 kudos

Pause a systick timer in cortex m3

Posted on December 02, 2017 at 17:29Is there a way to pause systick timer in cortex m3. Disabling/Enabling the timer doesn't pause it, but causes it to stop and restart. I want to pause the systick timer. Is there any way to do this?#systick #cortex...

STLink USB driver trouble on AC6 Eclipse

Posted on December 02, 2017 at 00:11Hello,I am facing a bug in AC6 SystemWorkbench STM32 software and I request you help. Being a total newbie on STM32, it is also highly probable that the corrective action is an evident one for more experienced use...

Resolved! SW enter HardFault_Handler using OpenStm32

Posted on December 01, 2017 at 04:30Hi,The project is developed with Keil MDK, it run well. But I use OpenStm32 to create one project, and copy the source code into the OpenStm32 project. I can run with ST Jlink V2, but the code enter HardFault_Hand...

0690X00000604HZQAY.jpg
kent gu by Associate III
  • 217 Views
  • 2 replies
  • 0 kudos

SW4STM32 external tool argument from user code

Posted on November 29, 2017 at 17:57Hi!I want to pass a string of my main.c as argument in an external tool in Eclipse (Run->External tools->External tools configuration).It's possible to pass, for example, the 'selected_text' (Returns the text curr...

Fib by Associate II
  • 121 Views
  • 0 replies
  • 0 kudos

question regarding map file stm32 & IAR

Posted on November 28, 2017 at 11:23The following 3 line are at the end of my map file produced by IAR.Does anyone know what the '(+ 976 absolute) ' part means?  15 550 bytes of readonly  code memory   1 088 bytes of readonly  data memory   3 020 by...

stm32 USB and simulink

Posted on November 25, 2017 at 06:04HelloI want use STM32-MAT/TARGET (simulink and stm32) but I need USB and it dont have USB block!How can I use USB in simulink?( STM32-MAT/TARGET )for example how can I send data with USB to other devices or how ca...

a m by Associate II
  • 151 Views
  • 0 replies
  • 1 kudos